SLVAFW0 December 2025 TPS61381-Q1
Figure 3-4 shows the placement of the power MOSFETs, input and output ceramic capacitors, main inductor, and the TPS61381-Q1 silicon on the top layer.
Output capacitors are placed adjacent to the VOUT pin of the TPS61381 external MOSFET source. The main inductor L1 is placed near the IL pin. The IL and SW nodes are poured with small copper plane to reduce the capacitive coupling relating to the SW node high dv/dt transitions. A large SW node copper plane helps the thermal, but can cause severe radiated emissions.