SLVAFW0 December 2025 TPS61381-Q1
Figure 3-6 shows an example of high side driver loop routing. Placing the bootstrap capacitor very close to the SW and the boot pins can reduce the gate loop enclosed areas. Route the gate drive traces from the silicon to the MOSFET as short as possible, routing the gate drive and the return traces side by side can minimize the gate-loop inductance and the gate-loop area.