SLVAFW0 December   2025 TPS61381-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2TPS61381-Q1 Schematic Guideline
    1. 2.1 GND Connection
    2. 2.2 Driver Design
    3. 2.3 IO Configuration
    4. 2.4 Output Capacitor
    5. 2.5 Compensation Design
      1. 2.5.1 Small Signal Analysis
      2. 2.5.2 Step by Step Loop Compensation Design
  6. 3TPS61381-Q1 Layout Guide Line
    1. 3.1 Identification of the Critical Switching Loops
      1. 3.1.1 Low Side Driver Loop
      2. 3.1.2 Boost Leg Switching Loop
      3. 3.1.3 High Side Driver Loop
    2. 3.2 Power Component Placement
    3. 3.3 Layout Example
      1. 3.3.1 Optimizing Low Side Driver Loop Example
      2. 3.3.2 Optimizing Boost Leg Switching Loop Example
      3. 3.3.3 Optimizing High Side Driver Loop Example
      4. 3.3.4 Signal Circuit Routing Example
  7. 4Summary
  8. 5References

Step by Step Loop Compensation Design

With the previous analysis on small signal models, we can calculate the compensation network parameters with the given inductor and output capacitor parameters. TI provides EXCEL calculation tools on designing compensation parameters. This section gives an example on calculating loop compensation with the design calculation tool.

  1. Set the Crossover Frequency, ƒC.

    The first step is to set the loop crossover frequency, ƒC. The higher the crossover frequency, the faster the loop response is. This is generally accepted that the loop gain crosses over no higher than the lower of either 1/10 of the switching frequency, ƒSW, or 1/5 of the RHPZ frequency, ƒzRHP.

  2. Set the Compensation Resistance, RCOMP.

    For a well compensated boost system, the fC is determined by RCOMP.Set your desired fC and the calculation tool can output recommended RCOMP.

     Set the Compensation
                            Resistance Figure 2-7 Set the Compensation Resistance

    The calculation tool recommends the Rout under these assumptions: For a properly designed boost system, ƒzCOMP must be placed below ƒC to make sure of phase margin. For common RCOMP range, RCOMP must be far smaller than the amplifier output resistance REA, which makes RCOMP | | REA ~ = RCOMP. Therefore, looking at Equation 6, the initial gain RCOMP × GCOMP × KFB is determined by RCOMP. Therefore the fc can be calculated by the equation that the close loop total gain T(s) = KPS(s) + HCOMP(s) is zero at ƒC.

    Equation 10. H C O M P = 20 l g G C O M P × R C O M P × R d o w n R u p + R d o w n = - K P S f c

    where

    • KPS is the gain of the power stage
    • GEA is the transconductance of the amplifier, the typical value of GEA = 24µS
  3. Set the Compensation Zero capacitor, CCOMP.

    The compensation zero needs to be placed at the power stage pole fpPS to compensate the phase drop near fpPS. Set ƒZ = ƒP, the CCOMP can be calculated . The calculation tool outputs the recommended CCOMP when the actual RCOMP is entered in line 80.

    Equation 11. C C O M P = R o u t × C o u t 2 R C O M P
     Set the Compensation
                            Capacitance Figure 2-8 Set the Compensation Capacitance
  4. Set the Compensation Pole Capacitor, CHF.

    The compensation pole needs to be placed to eliminate the ESR zero produced by RESR and Cout. Set ƒpCOMP2 = ƒzESR, and get:

    Equation 12. C H F = R E S R × C o u t R C O M P

    The recommended CHF is located at the calculation tool line 84 after the ESR and Cout is correctly entered in line 15-16.

     Set the Compensation
                            Capacitance Figure 2-9 Set the Compensation Capacitance
  5. Check Phase Margin and Gain Margin

    The calculated compensation parameters do not always make sure of stability, especially when the Cout has large ESR which bring fzESR into bandwidth. The calculation tool generates bode plot after all compensation parameters are entered. Check the bode plot for stability after steps 1-4. TI recommends phase margin > 60deg and gain margin > 10db. Reduce desired fc and re-calculate compensation in steps 1-4 if the margin does not meet requirements.

     Evaluate Loop
                            Stability Figure 2-10 Evaluate Loop Stability