SLVAFW0 December   2025 TPS61381-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2TPS61381-Q1 Schematic Guideline
    1. 2.1 GND Connection
    2. 2.2 Driver Design
    3. 2.3 IO Configuration
    4. 2.4 Output Capacitor
    5. 2.5 Compensation Design
      1. 2.5.1 Small Signal Analysis
      2. 2.5.2 Step by Step Loop Compensation Design
  6. 3TPS61381-Q1 Layout Guide Line
    1. 3.1 Identification of the Critical Switching Loops
      1. 3.1.1 Low Side Driver Loop
      2. 3.1.2 Boost Leg Switching Loop
      3. 3.1.3 High Side Driver Loop
    2. 3.2 Power Component Placement
    3. 3.3 Layout Example
      1. 3.3.1 Optimizing Low Side Driver Loop Example
      2. 3.3.2 Optimizing Boost Leg Switching Loop Example
      3. 3.3.3 Optimizing High Side Driver Loop Example
      4. 3.3.4 Signal Circuit Routing Example
  7. 4Summary
  8. 5References

Optimizing Low Side Driver Loop Example

According to the analysis in Figure 3-1, driver current must go through the net-tie before returning to VCC to reduce the length and enclosed areas of the low side driver current path. The net-tie between AGND and PGND must be connected between source of the low side MOSFET. Driver current return path is cut out from PGND copper and routed closely in parallel with the gate trace as differential pairs so that the mutual inductance can eliminate parasitic inductance. The VCC capacitor must be placed as close to the IC as possible.

 TPS61381-Q1 Low Side Driver
                    Layout Example Figure 3-5 TPS61381-Q1 Low Side Driver Layout Example