SLVSGS5A December 2023 – June 2024 DRV3946-Q1
PRODUCTION DATA
The DRV3946-Q1 is powered through the PVDD (12 V through an optional HS cut-off switch) and VDD (5 V) pins. While the drivers and the output stage are mainly supplied from PVDD, the logic, critical safety and diagnostic functions are driven from an internal 5V supply (safe 5V referred to as V5_S) that is derived from a power “OR” combination of PVDD and VDD. The power ORing ensures that the device maintains its intelligence and critical functions even if there is a loss of one of the supplies. Voltage references, current biases, oscillator and the digital block are powered by the V5_S. Redundant references and biases derived from PVDD are used to qualify V5_S and the oscillator.
Following a power-on-reset (POR) on V5_S, a power-up initialization is done that includes the address NAD determination, internal self-test (BIST) of the memory and diagnostics, RIPROPI determination and settling time for internal blocks within tREADY time. A CLR_FAULT SPI command from the user to acknowledge wake-up will place the device in the STANDBY state, with drivers in the high-impedance (Hi-Z) state until commanded by the user. The current consumption of the device will be IPVDD_STBY and IVDD_STBY in STANDBY state. Since the device uses a power "OR" architecture, certain functions are available even in the event that one of the external power supplies is lost.
Table 6-3 shows key device functionality with varying VDD voltage levels, assuming PVDD is within undervoltage and overvoltage limits.
| VDD | Relay-on (Active state) function | Off-state Diagnostics | SPI Communication |
|---|---|---|---|
| > VVDD_OV_RISE | Available(1) | Available(1) | SDI Ok, SDO will see VDD_ERR |
| Nominal | Available(1) | Available(1) | Available |
| < VVDD_UV_FALL | Available(1) | Available(1) | SDI Ok, SDO will see VDD_ERR |
Table 6-4 shows key device functionality with varying PVDD voltage levels, assuming VDD is within undervoltage and overvoltage limits.
| PVDD | Relay-on (Active state) function | Off-state Diagnostics | SPI Communication |
|---|---|---|---|
| > VPVDD_OV_RISE | Configurable with PVDD_OV_SHUTOFF_EN | Available(1) | Available |
| Nominal | Available(1) | Available(1) | Available |
| < VPVDD_UV_FALL | Device will go to STANDBY, outputs Hi-Z with QTO (passive) clamping, PVDD_UV flag will be set | Not Available | Available |
When PVDD < VPVDD_UV_FALL, transient behavior in the active-state during deglitch time is as follows:
If PVDD > VPVDD_UV_BIAS_FALL and internal regulation is enabled, device will switch to a 75% open loop regulation with fixed duty cycle and slew rate capped at SR = 0x2
If PVDD < VPVDD_UV_BIAS_FALL and internal regulation is enabled, device will switch to open loop regulation with 100% duty cycle
Table 6-5 shows key device functionality with loss of both PVDD and VDD power supplies.
PVDD | VDD | Relay-on (Active state) function | Off-state diagnostics | SPI communication |
< VPVDD_RST_FALL | < VVDD_RST_FALL | Not available | Not available | Not available |