SLVSGS5A December 2023 – June 2024 DRV3946-Q1
PRODUCTION DATA
The device has two dedicated pins for secondary shut off to Hi-Z the driver. Both pins have an internal pull-down resistance to GND. PIN_CONFIG settings determines the function of the two pins as summarized below.
EN/EN1 | DIS/EN2 | PIN_CONFIG = 0x0 | EN/EN1 | DIS/EN2 | PIN_CONFIG = 0x1 |
Lo | Lo | Both outputs Hi-Z | Lo | Lo | Both outputs Hi-Z |
Lo | Hi | Both outputs Hi-Z | Lo | Hi | Output 1 Hi-Z, Output 2 controlled by SPI CMD |
Hi | Lo | Both outputs controlled by SPI CMD | Hi | Lo | Output 1 controlled by SPI CMD, Output 2 Hi-Z |
Hi | Hi | Both outputs Hi-Z | Hi | Hi | Both outputs controlled by SPI CMD |
With PIN_CONFIG = 0b (default), EN/EN1 pin has to be driven high externally to turn ON the drivers, but DIS/EN2 pin can be left floating if not needed.
For pin triggered turn-on or turn-off, the user can program a delay before the request is processed using the CHx_PIN_TURNON_DLY and CHx_PIN_TURNOFF_DLY.