SLVSIR8 June 2026 TPS61383-Q1
PRODUCTION DATA
With the previous analysis on small signal models, calculate the compensation network parameters with the given inductor and output capacitor parameters. This section gives an example on calculating loop compensation.
The first step is to set the loop crossover frequency, ƒC. The higher the crossover frequency, the faster the loop response is. The loop gain crosses over no higher than the lower of either 1/10 of the switching frequency, ƒSW, or 1/5 of the RHPZ frequency, ƒzRHP.
For a well compensated boost system, the fC is determined by RCOMP. For a properly designed boost system, ƒzCOMP is placed below ƒC to keep phase margin. And for common RCOMP range, RCOMP is far smaller than the amplifier output resistance REA, which makes RCOMP | | REA ≅ RCOMP. Therefore, in the following equation, the initial gain RCOMP × GCOMP × KFB is determined by RCOMP. Therefore, the fc is calculated by the equation that the close loop total gain T(s) = KPS(s) + HCOMP(s) is zero at ƒC.
where
The compensation zero is placed at the power stage pole fpPS to compensate the phase drop near fpPS. Set ƒZ = ƒP, the CCOMP is calculated as:
The compensation pole is placed to eliminate the ESR zero produced by RESR and Cout. Set ƒpCOMP2 = ƒzESR, and get:
The calculated compensation parameters does not always mean stability, especially when the Cout has big ESR which bring fzESR into bandwidth. TI provides an excel calculation tool which generates bode plot after all compensation parameters are selected. Check the bode plot for stability after steps 1 – 4. TI recommends phase margin > 60deg and gain margin > 10db. Reduce desired fc and re-calculate compensation in steps 1 – 4 if the margin does not meet requirements.