SLVSIR8 June 2026 TPS61383-Q1
PRODUCTION DATA
The capacitance in the backup battery side affects BUB loop stability. Select the effective capacitance between 5μF to 10μF if BUB loop functions needs to be applied. If BUB loop function is not required, then the capacitance in the BUB side does not have upper limit.
Care needs to be taken when evaluating the effective capacitance of a ceramic capacitor. For ceramic capacitors, the derating under dc bias voltage, aging, and AC signal must be taken into consideration. Taking Murata GCM21BR71C475KA73K as an example, the effective capacitance reduces by 56% when 8V DC voltage is applied.
If backup battery is connected to the IC through long cable, TI recommend adding extra 100 – 200uF electrolytic capacitors on the BUB side. This capacitor helps suppress LC ringing caused by parasite inductance on backup battery cable. Note that the electrolytic capacitor does not replace ceramic capacitor and 5μF to 10μF ceramic capacitors still must be placed near the IC.