SLVUCJ9 February 2023 LP8764-Q1 , TPS6594-Q1
The TPS65941120 GPIO8 is configured as an input to disable the watchdog. Typically, during development this pin is tied high, so that when the nRSTOUT bit is set WD_PWRHOLD is also set. The configuration of this pin can be utilized for other features or functions but this requires servicing the watchdog before it expires. The watchdog long window is 772 seconds, Table 5-13.
Write 0x12:0x09:0x00:0xBF // Disable Watchdog
Write 0x48:0x38:0x01:0x00 // configure GPIO8 as a pushpull output
When it is time to enable and configure the watchdog, then in addition to enabling the watchdog the WD_PWR_HOLD must be cleared.
Write 0x12:0x09:0x00:0xFB // Clear WD_PWRHOLD
Write 0x12:0x09:0x40:0xBF // Enable Watchdog
In addition to the GPIO8 of the TPS65941120 there are also the feedback pins for BUCK4 on the TPS65941120. This monitor can be used independently since the BUCK4 regulator is multiphased with BUCKs 1, 2 and 3. When enabling a monitor, the built in self-test is performed. Please refer to the data sheet for an explanation of the monitor self-test. If the self-test fails this results in a Moderate error that triggers the TO_SAFE_ORDERLY power sequence.
Unlike the GPIO, the BUCK monitor can become part of the PFSM by assigning a group to the BUCK regulator and unmasking the OV/UV interrupts. Per Table 5-7, the BUCK4_GRP_SEL is not assigned a group.
| Selected Rail group Selection | PFSM Trigger | Description |
|---|---|---|
| No Group Assigned | None | OV/UV can set nINT pin for MCU interrogation. |
| MCU Rail Group | MCU Power Error | OV/UV can trigger TO_SAFE |
| Soc Rail Group | SoC Power Error | OV/UV can trigger |
| Other Rail Group | Orderly Shutdown | OV/UV can triggerTO_SAFE_ORDERLY |
In this example BUCK4 is used to monitor a 0.8V supply. The wait statement ensures that the built in self-test of the monitors is completed before the OV and UV monitors are unmasked. Refer to the TPS6594-Q1Power Management IC (PMIC) with 5 Bucks and 4 LDOs for Safety-Relevant Automotive Applications data sheet for more details.
Write 0x48:0x14:0x37:0x00 // Set to 0.8V
Write 0x48:0x0B:0x07:0xF1 // Set slew rate to 0.31mV/us
Write 0x48:0x41:0xA0:0x0F // SOC rail group
Write 0x48:0x4A:0x30:0xCF // Mask OV/UV
Write 0x48:0x0A:0x10:0xEF // Enable BUCK4 Monitor
// Startup = 220us, ramp = 42us, settling = 105us, OV/UV test=50us
wait 500us
Write 0x48:0x4A:0x00:0xCF // Unmask OV/UV
With the TO_SAFE and TO_SAFE_ORDERLY sequences the PMICs transition through the SAFE RECOVERY state as well as hardware states INIT and BOOT BIST. Through this transition the user registers are restored with the NVM settings. For both the GPIO and BUCK monitor customizations, these customizations are not preserved and must be re-applied with every power cycle and transition through the hardware states.