SLVUD17B February 2025 – November 2025
The Register Map page (shown in Figure 3-8) lists the different registers available for configuration and is intended for direct reads and writes to the PMIC registers. Reading and writing registers can be done individually or all at once. Enable an Auto Read feature by using the drop-down menu next to the READ ALL REGISTERS button to select an automatic read timing. Use the search bar at the top of the page to search registers by name or address.
The first three columns under the search bar show the name of each register, followed by the hexadecimal address and data value. The Bits column contains the bit values for each register and can be hidden by unchecking the Show Bits box at the top of the page, under the READ ALL REGISTERS button. Double-clicking a bit in this section changes the bit value.
The Field View section on the right side of the page shows register bits grouped by the respective control blocks. Select the question mark icon next to the bit field label for an expanded view with more detail on the bit field. This function also highlights the corresponding bit boxes in yellow in the Bits column. Each field has a name shown by the blue text at the top of each box. Find the field names by using the search bar by checking the Search Bitfields box to the right of the search bar.
In the Immediate Write mode (toggle option located at the top right of the page), write buttons are grayed out because the individual registers are written immediately with each change in the Field View, change in bits, or change in hexadecimal value. In Deferred Write mode, the writing of a single register or all registers is deferred until the WRITE REGISTER or WRITE ALL REGISTERS button is selected.
Figure 3-8 Register Map PageRead-only registers are grayed out and locked to prevent write attempts. Reserved register bits are shown as a dash mark.