SLVUD67 September 2025 TPS6521505-Q1
The TPS6521505 has the default I2C address configured as 0x30. This configuration can be changed if needed by searching for register I2C_ADDRESS_REG in the register map of the TPS65215-GUI and changing the default 0x30 address as shown in Figure 5-10. Since any write to this register has immediate reaction, you must change the Device I2C address to the new value as shown in Figure 5-11. Once the register is changed, the new value must be saved into the NVM by writing 0x0A to register 0x34. The device now starts communicating with the new address set in Device I2C address.
| Register Address | Bit | Field Name |
|---|---|---|
| 0x26 | 6-0 | I2C_ADDRESS_REG |