SLVUD67 September 2025 TPS6521505-Q1
There are several interrupt settings that can be masked to bypass specific PMIC monitoring features or modify how PMIC reacts when interrupts are detected. The interrupts that can be masked include undervoltage monitoring, temperature monitoring, among others. Figure 5-10 shows the mask settings in the configuration tab of the GUI.
| Register Address | Bit | Field Name |
|---|---|---|
| 0x1E | 7 | BYPASS_RAILS_DISCHA RGED_CHECK |
| Register Address | Bit | Field Name |
|---|---|---|
| 0x24 | 7 | MASK_RETRY_COUNT |
| 6 | BUCK3_UV_MASK | |
| 5 | BUCK2_UV_MASK | |
| 4 | BUCK1_UV_MASK | |
| 2 | LDO2_UV_MASK | |
| 0 | LDO1_UV_MASK |
| Register Address | Bit | Field Name |
|---|---|---|
| 0x25 | 7 | MASK_INT_FOR_PB |
| 6-5 | MASK_EFFECT | |
| 4 | MASK_INT_FOR_RV | |
| 3 | SENSOR_0_WARM_MASK | |
| 2 | SENSOR_1_WARM_MASK | |
| 1 | SENSOR_2_WARM_MASK | |
| 0 | SENSOR_3_WARM_MASK |