Once the register settings are
updated, the new values can be saved into the NVM by writing 0x0A to register
address 0x34.
- Figure 5-2 shows the button that saves the register settings into the NVM when using the
TPS65215-GUI.
- Table 5-22 shows the register field to be written when NOT using the TPS65215-GUI.
Table 5-22 I2C Write to Save Register
Settings into NVM
| Register Address |
Bit |
Field Name |
Data |
| 0x34 |
3-0 |
USER_NVM_CMD |
0x0A |
Note: It is recommended to export the
selected register settings into a CSV and JSON file using the TPS65215-GUI.
Figure 5-14 shows how to export the NVM settings. The file format must be selected on
"Register File Format" before using the "Save Registers As".