SLVUDA2 July 2025
Figure 2-6 shows circuit for Configuration 2 and Table 2-5 outlines the header pin settings.
This use case sets the reference voltage to mid-supply for REFA and REFB. The voltage is set by channel A of the external reference buffer (U2). The buffer circuitry must be populated and at a minimum, the following components must be added: U2, R6, R7, R8, R9, R10, R11, R12, R13. In this circuit, both REFA and REFB are biased by the same voltage by shorting J12. The corresponding transfer function becomes Equation 2, where the output of the reference buffer is VREF.
| HEADER NAME | SETTING |
|---|---|
| J12 | Open |
| J13 | Closed (REFA to OPA) |
| J14 | Open |