SLYY228 November   2024

 

  1.   1
  2.   Introduction
  3.   Basics of USB Type-C®
    1.     Abstract
    2.     USB-C data speeds and power levels
    3.     Data and power roles
    4.     USB-C pinout and reversibility
    5.     USB-C cable detection and orientation
    6.     When do you need a USB PD controller?
  4.   History of USB Type-C®
    1.     Abstract
    2.     USB connector basics
    3.     USB and USB PD protocol history
    4.     USB-C vs. USB PD
    5.     Evolution of the USB PD 3.1 specification
  5.   Introduction and Overview of the USB Type-C® and USB PD Specifications
    1.     Abstract
    2.     USB-C connections
    3.     VCONN and messaging types
    4.     Negotiating USB PD power over CC wires
    5.     Data-role swaps
    6.     Power-role swaps
    7.     Introduction to USB PD alternate mode
    8.     Introduction to EPR
  6.   USB signals over USB Type-C®
    1.     Introduction
    2.     USB 2.0 Signaling Over Type-C
    3.     Low speed and full speed
    4.     High speed
    5.     Low-, full- and high-speed data rates
    6.     USB 2.0 signal integrity
    7.     SuperSpeed Signaling over USB-C
    8.     SuperSpeed startup speed negotiation
    9.     SuperSpeed signal integrity challenges
  7.   Signal Multiplexing for USB Type-C®
    1.     USB-C USB 2.0
    2.     USB-C USB 3
    3.     USB PD DisplayPort™ alternate mode multiplexing
    4.     DisplayPort source device (DFP_D) pin assignment C
    5.     DisplayPort source device (DFP_D) pin assignment D
    6.     DisplayPort source device (DFP_D) pin assignment E
    7.     DisplayPort sink device (UFP_D) pin assignment C
    8.     DisplayPort sink device (UFP_D) pin assignment D
    9.     DisplayPort sink device (UFP_D) pin assignment E
  8.   USB4
    1.     USB4 Overview
    2.     USB4 discover and entry process
    3.     USB4 System
    4.     Sideband Communication
    5.     USB4 lanes and data rates
    6.     Loss Budget
    7.     Supporting DisplayPort Alternate Mode and USB4 over SBU1 and SBU2
  9.   Introduction to eUSB2
    1.     Abstract
    2.     eUSB2 overview
    3.     eUSB2 modes
    4.     Other features
  10.   Extended Power Range (EPR)
    1.     Abstract
    2.     What is EPR?
    3.     Technical specifications
    4.     Safety implications >100W
    5.     Handling power negotiation with TI’s PD controllers
    6.     Conclusion
  11.   USB Type-C® and USB power delivery common use cases and block diagrams
    1.     5V USB-C source-only port (no USB PD)
    2.     Basic functional blocks
    3.     5V USB-C source-only port with USB 3.0 data (no USB PD)
    4.     5V USB-C sink-only port (no USB PD)
    5.     5V USB-C DRP (no USB PD)
    6.     20V USB-C source-only port with USB PD
    7.     20V USB-C sink-only port with USB PD
    8.     5V source, 20V sink USB-C port with USB PD and DisplayPort™ Alternate Mode
    9.     20V USB-C DRP with USB PD and a battery charger
  12.   End equipment-specific block diagrams
    1.     Abstract
    2.     Laptops and industrial PCs
    3.     Docking station
    4.     Bluetooth® speaker
    5.     Wi-Fi® routers and smart speakers
    6.     Power tools
  13.   Benefits of a TI PD Controller
    1.     Abstract
    2.     TI solutions to common design challenges
      1.      TI offers highly integrated solution
      2.      TI offers simple configuration tool
      3.      TI products are rigorously validated and USB-IF certified
    3.     Other benefits of using TI PD controllers
      1.      TI offers complete reference design
      2.      TI offers great customer support
      3.      Conclusion

5V source, 20V sink USB-C port with USB PD and DisplayPort™ Alternate Mode

In a notebook or PC implementation, a single USB-C port has the ability to sink USB PD voltages in order to charge the battery; provide at least 5V out to power small connected devices such as mice, keyboards and flash drives; and connect a monitor. You can quickly see how the required capabilities of a USB-C port is robust and flexible enough to meet the end user’s expectations for certain end equipment.

Figure 50 shows the power architecture for this type of system. There are typically separate power paths in the system: one for sourcing the 5V and another for sinking up to 20V. If you only have one USB-C port in the system, you could implement a single power path rather than two separate ones. In such cases, you would need the battery charger to have bidirectional support, and include on-the-go support. Most systems that require 5V source and 20V sink as well as DisplayPort Alternate Mode support will have more than one USB port.

 5V source 20V sink USB PD
                    block diagram Figure 50 5V source 20V sink USB PD block diagram

If the end equipment will have multiple USB ports, a shared 5V rail can provide the sourcing power for both USB Type-A and USB-C ports. You will need to calculate the power budget of this 5V DC/DC supply based on the maximum current supported by each USB port when sourcing 5V to connected devices.

Connecting the sink power path to the battery charger isolates the capacitance from the battery charger from VBUS, while also making sure that the battery charger receives power when the user connects an AC/DC adapter.

As in the previous examples, the USB PD controller will have integrated power path or provide a method to control them through GPIOs. Some USB PD controllers offer a N-channel field-effect transistor (NFET) gate driver to drive external NFETs directly.

Figure 50 also shows that the USB PD controller has the ability to supply VCONN. The USB PD source-only design requires VCONN when exceeding 3A of current. But adding support for DisplayPort Alternate Mode requires VCONN in order to determine the data capabilities of the cable, not the power capabilities. Similar to the 5V USB-C source-only port with USB 3.0 data example, it’s important to confirm that the connected cable has capabilities for supporting DisplayPort Alternate Mode as well. VCONN needs to power the e-marker in the cable in order to read back its capabilities.

Figure 51 shows a more complete block diagram that includes both the power and data blocks for implementing a 5V source, 20V sink USB-C port with USB PD and DisplayPort™ Alternate Mode design.

The last block in Figure 51 is the DisplayPort Alternate Mode multiplexer. As in previous cases, DisplayPort Alternate Mode also uses the SuperSpeed pins on the USB-C connector to transmit video data.

 5V source 20V sink with
                    DisplayPort™ USB PD block diagram Figure 51 5V source 20V sink with DisplayPort™ USB PD block diagram

DisplayPort Alternate Mode includes several different pin configurations that help determine the distribution of the SuperSpeed pins between supporting USB 3.0 or DisplayPort video data. There are pin configurations that enable maximum bandwidth for DisplayPort by dedicating all SuperSpeed pairs for DisplayPort, and pin configurations that split the SuperSpeed pairs to enable both USB 3.0 and DisplayPort data simultaneously. The DisplayPort specification has further details about the pin configurations supported on USB-C.

The DisplayPort Alternate Mode multiplexer will multiplex the SuperSpeed pins to either the DisplayPort host or USB host, depending on the pin assignment negotiated within DisplayPort Alternate Mode. As with other peripheral devices, the USB PD controller is expected to communicate over I2C or with GPIOs to the DisplayPort Alternate Mode multiplexer to configure it accordingly. If the port partner also supports DisplayPort Alternate Mode, the USB PD controller will automatically negotiate and enter DisplayPort Alternate Mode with the connected device. Based on this negotiation, the USB PD controller will then configure the DisplayPort Alternate Mode multiplexer through either I2C or GPIO. During USB PD negotiation, power always gets negotiated first, followed by alternate modes such as DisplayPort.