SLYY228 November 2024
Historically, battery powered end-equipment has used either a barrel jack, coaxial cable or proprietary cable to charge the product. Moving to USB-C with USB PD enables you to both source and sink power, which then enables the conversion of a battery-powered device to a power bank. In other words, end users can both charge connected devices through USB-C and also have a device charged through the same USB-C connector. To accomplish these requirements, you would likely implement a DRP architecture with a bidirectional battery charger. Although this implementation may sound complex, it is typically a two-chip self-contained solution.
Figure 52 is a block diagram for a 20V USB DRP with USB PD design leveraging a bidirectional battery-charger IC. In this case, the battery charger charges the batteries when the end user connects a charger device. The battery charger will also provide the correct voltage on VBUS when the end user connects a device that needs charging. In this case, the USB PD controller will also communicate to the charger IC over I2C. When operating as a power source, the USB PD controller will communicate to the battery charger whether there’s a connection, what voltage to provide, and where to set the current limit. The battery charger will need to have the correct voltage to meet the tolerances of the USB PD specification, and also ensure the voltage transitions (from 5V to 20V, for example) to meet the timing requirements of the USB PD specification. Typically, if a battery charger is designed for USB PD applications, it would be designed to meet those specifications, or provide configurable settings to adjust the voltage transitions in order to tune the output for USB PD compliance.
Figure 52 5V source 20V sink USB PD
block diagramWhen operating as a power sink, the USB PD controller will communicate what power is available to the battery charger and enable the battery charger to start charging the battery. Figure 52 includes an additional 20V DRP power path because most battery charger ICs will require more than 10µF of capacitance on the input pin for stability. If you plan to use a charger IC that can operate with less than 10µF of capacitance, you can remove the 20V DRP power path from the system.