SLYY228 November 2024
Power tools and similar portable power packs to power and charge laptops, phones and speakers on the go are another type of end equipment adopting USB-C. Figure 59 and Figure 60 show typical block diagrams for these types of systems.
Figure 59 Power tools block diagram
1
Figure 60 Power tools block diagram
2While many designers are converting all of their USB Type-A ports to USB-C ports, some end equipment continues to include the older technology in order to power their customers’ older products. One example of this is with power tools. Like Bluetooth speakers, the power tool battery pack has the ability to source and sink power from a single USB-C port. The USB Type-A port would only source power to charge connected devices.
There are two different implementations from a power perspective:
Another similarity between a power tool and a Bluetooth speaker is that the main reason to chose one topology over another is predicated on the output voltage on the USB-C port. If the USB-C port only needs a maximum of 5V, then a shared DC/DC topology may be the most beneficial, with the battery charger that’s tied to the USB-C port acting only as a power sink. If the USB-C port is expected to supply >5V, then having the battery charger act as both the source and sink, relying on the on-the-go functionality built into the charger, is likely the best path forward.