SLYY228 November   2024

 

  1.   1
  2.   Introduction
  3.   Basics of USB Type-C®
    1.     Abstract
    2.     USB-C data speeds and power levels
    3.     Data and power roles
    4.     USB-C pinout and reversibility
    5.     USB-C cable detection and orientation
    6.     When do you need a USB PD controller?
  4.   History of USB Type-C®
    1.     Abstract
    2.     USB connector basics
    3.     USB and USB PD protocol history
    4.     USB-C vs. USB PD
    5.     Evolution of the USB PD 3.1 specification
  5.   Introduction and Overview of the USB Type-C® and USB PD Specifications
    1.     Abstract
    2.     USB-C connections
    3.     VCONN and messaging types
    4.     Negotiating USB PD power over CC wires
    5.     Data-role swaps
    6.     Power-role swaps
    7.     Introduction to USB PD alternate mode
    8.     Introduction to EPR
  6.   USB signals over USB Type-C®
    1.     Introduction
    2.     USB 2.0 Signaling Over Type-C
    3.     Low speed and full speed
    4.     High speed
    5.     Low-, full- and high-speed data rates
    6.     USB 2.0 signal integrity
    7.     SuperSpeed Signaling over USB-C
    8.     SuperSpeed startup speed negotiation
    9.     SuperSpeed signal integrity challenges
  7.   Signal Multiplexing for USB Type-C®
    1.     USB-C USB 2.0
    2.     USB-C USB 3
    3.     USB PD DisplayPort™ alternate mode multiplexing
    4.     DisplayPort source device (DFP_D) pin assignment C
    5.     DisplayPort source device (DFP_D) pin assignment D
    6.     DisplayPort source device (DFP_D) pin assignment E
    7.     DisplayPort sink device (UFP_D) pin assignment C
    8.     DisplayPort sink device (UFP_D) pin assignment D
    9.     DisplayPort sink device (UFP_D) pin assignment E
  8.   USB4
    1.     USB4 Overview
    2.     USB4 discover and entry process
    3.     USB4 System
    4.     Sideband Communication
    5.     USB4 lanes and data rates
    6.     Loss Budget
    7.     Supporting DisplayPort Alternate Mode and USB4 over SBU1 and SBU2
  9.   Introduction to eUSB2
    1.     Abstract
    2.     eUSB2 overview
    3.     eUSB2 modes
    4.     Other features
  10.   Extended Power Range (EPR)
    1.     Abstract
    2.     What is EPR?
    3.     Technical specifications
    4.     Safety implications >100W
    5.     Handling power negotiation with TI’s PD controllers
    6.     Conclusion
  11.   USB Type-C® and USB power delivery common use cases and block diagrams
    1.     5V USB-C source-only port (no USB PD)
    2.     Basic functional blocks
    3.     5V USB-C source-only port with USB 3.0 data (no USB PD)
    4.     5V USB-C sink-only port (no USB PD)
    5.     5V USB-C DRP (no USB PD)
    6.     20V USB-C source-only port with USB PD
    7.     20V USB-C sink-only port with USB PD
    8.     5V source, 20V sink USB-C port with USB PD and DisplayPort™ Alternate Mode
    9.     20V USB-C DRP with USB PD and a battery charger
  12.   End equipment-specific block diagrams
    1.     Abstract
    2.     Laptops and industrial PCs
    3.     Docking station
    4.     Bluetooth® speaker
    5.     Wi-Fi® routers and smart speakers
    6.     Power tools
  13.   Benefits of a TI PD Controller
    1.     Abstract
    2.     TI solutions to common design challenges
      1.      TI offers highly integrated solution
      2.      TI offers simple configuration tool
      3.      TI products are rigorously validated and USB-IF certified
    3.     Other benefits of using TI PD controllers
      1.      TI offers complete reference design
      2.      TI offers great customer support
      3.      Conclusion

USB4 System

The USB4 system comprises a host, hub device, peripheral device and dock, each of which contain a router. The router maps tunneled protocol traffic to USB4 packets and routes packets through the USB4 fabric. Figure 31 shows the block diagrams for a USB4 host, hub, and device.

 USB4 Host, Hub, and Device Figure 31 USB4 Host, Hub, and Device

The host contains the host router, an USB host controller (both USB3.2 and USB2), and a DisplayPort source. The host may have more than one DFP. The host may optionally incorporate a PCIe controller or PCIe switch if PCIe tunneling is supported. Residing in a host is the connection manager software, which enumerates, configures and manages the entire USB4 domain. Figure 32 takes a closer look at a USB4 hub.

 USB4 Hub Figure 32 USB4 Hub

A hub has a single upstream-facing port (UFP) and, like a host, can have more than one DFP. A hub router supports USB2, USB3, a PCIe switch and DisplayPort™ tunneling. Figure 33 takes a closer look at a USB4 peripheral device.

 USB4 Peripheral Device Figure 33 USB4 Peripheral Device

A peripheral device has a single UFP and no DFP, and may optionally contain one or more enhanced SuperSpeed hubs, enhanced SuperSpeed functionality, PCIe switches or endpoints, or DisplayPort source or sink functionality. Figure 34 takes a closer look at a USB4 dock

 USB4 Dock Figure 34 USB4 Dock

A USB4 dock is similar to a USB4 hub with a single UFP and one or more DFPs. Unlike a USB4 hub, the dock contains one or more protocol adapters such as DisplayPort.

All USB4 components connect using USB-C passive or active cables in a spanning tree with the host at the top, a hub in the middle and a peripheral device at end of tree. There can be as many as five hubs between the host and the peripheral router. All of these products are configured using a sideband channel.