SNIS238 July 2025 TMP9R01-SEP
PRODUCTION DATA
The TMP9R01-SEP device supports reset using the two-wire general-call address 00h (0000 0000b). The TMP9R01-SEP device acknowledges the general-call address and responds to the second byte. If the second byte is 06h (0000 0110b), the TMP9R01-SEP device executes a software reset as shown in Figure 7-9. This software reset restores the power-on reset state to all TMP9R01-SEP registers and aborts any conversion in progress. The TMP9R01-SEP device takes no action in response to other values in the second byte.