Remote temperature sensing on the TMP9R01-SEP device measures very small voltages using very low currents; therefore, noise at the device inputs must be minimized. Most applications using the TMP9R01-SEP have high digital content, with several clocks and logic-level transitions that create a noisy environment. Layout must adhere to the following guidelines:
- Place the TMP9R01-SEP device as close to the remote junction sensor as possible.
- Route the D+ and D– traces next to each other and shield them from adjacent signals through the use of ground guard traces, as shown in Figure 9-4. If a multilayer PCB is used, bury these traces between the ground or V+ planes to shield them from extrinsic noise sources. 5mil (0.127mm) PCB traces are recommended.
- Minimize additional thermocouple junctions caused by copper-to-solder connections. If these junctions are used, make the same number and approximate locations of copper-to-solder connections in both the D+ and D– connections to cancel any thermocouple effects.
- Use a 0.1μF local bypass capacitor directly between the V+ and GND of the TMP9R01-SEP device. For optimum measurement performance, minimize filter capacitance between D+ and D– to 1000pF or less. This capacitance includes any cable capacitance between the remote temperature sensor and the TMP9R01-SEP device.
- If the connection between the remote temperature sensor and the TMP9R01-SEP device is less than 8in (20.32cm) long, use a twisted-wire pair connection. For lengths greater than 8 in, use a twisted, shielded pair with the shield grounded as close to the TMP9R01-SEP device as possible. Leave the remote sensor connection end of the shield wire open to avoid ground loops and 60Hz pickup.
- Thoroughly clean and remove all flux residue in and around the pins of the TMP9R01-SEP device to avoid temperature offset readings as a result of leakage paths between D+ and GND, or between D+ and V+.