SNVSCM0A June 2025 – October 2025 LM51772-Q1
PRODUCTION DATA
The LM51772-Q1 is designed to operate over a wide input voltage range. The device is not allowed to be operated with an input supply, which characteristics are not compatible with the Absolute Maximum Ratings and Recommended Operating Conditions. Select, a input supply that is capable of delivering the required input current to the fully loaded regulator. Use Equation 66 to estimate the average input current.
where
If the device is connected to an input supply through long wires or PCB traces with a large impedance, take special care to achieve stable performance. The parasitic inductance and resistance of the input cables possible have an adverse effect on converter operation. The parasitic inductance in combination with the low-ESR ceramic input capacitors form an under-damped resonant circuit. In some cases this circuit cause overvoltage transients at VIN each time the input supply is cycled ON and OFF. The parasitic resistance causes the input voltage to dip during a load transient. One way to solve such issues is to reduce the distance from the input supply to the regulator and use an aluminum or tantalum input capacitor in parallel with the ceramics. The moderate ESR of the electrolytic capacitors helps to damp the input resonant circuit and reduce any voltage overshoots. An EMI input filter is often used in front of the controller power stage. Unless carefully designed, the filter has the potential to lead to instability as well as some of the previously mentioned affects.