SPMU447 June 2026 CC2755P20
Any sectors that should not be modified during runtime by either the SSB or the application should be write/erase-protected via the ccfg.flashProt.writeEraseProt fields.
Any sectors that should not be readable during runtime by either the SSB or the application should be read-protected via the ccfg.flashProt.readProt fields.
At a minimum, the CCFG and SCFG sectors should be write/erase-protected.
If there is a desire to protect from chip erase, and if chip erase is allowed (see Section 10.1.4), then configure ccfg.flashProt.chipEraseRetain accordingly.