SPMU447 June 2026 CC2755P20
Controllers (devices that generate bus transactions) other than the main CPU have a gasket that may block transactions from the controller to NSC marked memory. By default, controllers are not blocked. If this gasket is enabled through a signal from TCM, then transactions where A[28]=0 are blocked. A blocked read transaction will cause an error indication to the controller and will return data as 0x0. A blocked write transaction will cause an error to the controller. Blocked transactions do not propagate on the bus past the gasket.
Non-CPU controllers will also have a periphery port for control. This periphery port is secured independently from the controller port and has a gasket just like any other periphery.