SPMU447 June 2026 CC2755P20
The serial audio interface consists of two or three clock signals and one or two data signals(AD0,AD1), depending on how the I2S module is used. The clock signals(MCLK,BCLK,WCLK) can be generated either internally (by the PRCM module) or externally (by the audio device or another clock source).
The ADx pins cannot be dynamically placed in a tristate condition. Therefore, TDM mode is supported for ADx input pins where only external audio devices drive these signals, but TDM mode is not supported for ADx output pins.