SPMU447 June 2026 CC2755P20
The sampling clock source is selected in the CKMD module using the SRC bits in the ADCCLKSEL register.
The desired sampling period for ADC operation can be generated using the internal clock divider and/or the sample timer, which applies to the AUTO sampling mode. The internal clock divider is configured using the SCLKDIV bits in the CTL0 register and has divide options of 1, 2, 4, 8, 16, 24, 32, and 48.
The duration of the sampling period can be programmed to one of two user-defined values set by the SCOMP0 and SCOMP1 sample timer registers. The value in SCOMPx configures the sampling period by defining the number of sample time clocks to set the sample window to. The default SCOMPx sample timer value translates to 1-cycle-wide sample pulse, which allows the sampling period to be solely based on the sample clock and SCLKDIV. In general, there are three parameters that can be used to control the sample period: SCOMPx, SCLKDIV, and the source of the sample clock.
When the AUTO power down mode is selected using PWRDN=0, the module enables the signal to the ADC peripheral to be generated one sampling clock cycle after the sample signal is asserted. This should be considered by the user in the sample window calculation, in addition to the ADC power time or settling time needs of other analog modules such as the Temperature Sensor, VREF, and so on.