SPMU447 June 2026 CC2755P20
All fault exceptions other than HardFault have a configurable exception priority. Software can disable execution of the handlers for these faults.
Usually, the exception priority and the values of the exception mask registers determine whether the processor enters the fault handler. They also determine if one fault handler can preempt another.
In some situations, a fault with configurable priority is treated as a HardFault. This is called priority escalation, and the fault is described as escalated to HardFault. Escalation to HardFault occurs when:
A fault handler causes the same kind of fault as the one it is servicing. This escalation to HardFault occurs because a fault handler cannot preempt itself; it must have the same priority as the current execution priority level.
A fault handler causes a fault with the same or lower priority as the fault it is servicing. This is because the handler for the new fault cannot preempt the currently executing fault handler.
An exception handler causes a fault for which the priority is the same as or lower than the currently executing exception.
A fault occurs, and the handler for that fault is not enabled.
If a BusFault occurs during a stack push when entering a BusFault handler, the BusFault does not escalate to a HardFault. This means that if a corrupted stack causes a fault, the fault handler executes even though the stack push for the handler failed. The fault handler operates but the stack contents are corrupted.
BusFaults and fixed priority exceptions can be designated as Secure or Non-secure under the control of SCB:AIRCR.BFHFNMINS. When AIRCR.BFHFMNINS is set to:
0: BusFaults and fixed priority exceptions are designated as Secure. The exceptions retain the prioritization of HardFault at -1 and NMI at -2.
1: BusFaults and fixed priority exceptions are designated as Non-secure. In this case, Secure HardFault is introduced at priority -3 to ensure that faults that target Secure state are recognized.
The Non-secure state cannot inhibit BusFaults and fixed priority exceptions that target Secure state. Therefore, when faults and fixed priority exceptions are Secure, Non-secure FAULTMASK (FAULTMASK_NS) only inhibits programmable priority exceptions, making it equivalent to Non-secure PRIMASK (PRIMASK_NS).
Non-secure programmable priority exceptions are mapped to the regular priority range 0-255 if SCB:AIRCR.PRIS is clear. Non-secure programmable priority exceptions are mapped to the bottom half of the regular priority range, 128-255, if AIRCR.PRIS is set to 1. Therefore, the FAULTMASK_NS sets the execution priority to 0x0 or 0x80, according to AIRCR.PRIS, to mask the Non-secure programmable priority exception only.
When BusFaults and fixed priority exceptions are Secure, FAULTMASK_S sets execution priority to -1 to inhibit everything up to and including HardFault.
When BusFaults and fixed priority exceptions are designated as Non-secure, FAULTMASK_NS boosts priority to -1 to inhibit everything up to Non-secure HardFault at priority -1, while FAULTMASK_S boosts priority to -3 to inhibit all faults and fixed priority exceptions, including the Secure HardFault at priority -3.
Only Reset can preempt the fixed priority Secure HardFault when SCB:AIRCR.BFHFNMINS is set to 1. A Secure HardFault when AIRCR.BFHFNMINS is set to 1 can preempt any exception other than Reset.
A Secure HardFault when AIRCR.BFHFNMINS is set to 0 can preempt any exception other than Reset, NMI, or another HardFault.