SPRABJ8E September 2022 – November 2026 AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The 3.3V power system on AM26x ZCZ devices are explored using the AM263x controlCARD EVM (TMDSCNCD263), from the 3.3V buck-converter (TPS62913RPUR, U30) through the board power planes and ending in at the BGA bulk and per pin decoupling capacitor array. A common buck-converter supplies power for all of the AM263x digital I/O, analog I/O and the rest of the controlCard 3.3V loads. This is common in most designs where all 3.3V digital level I/O share a common power supply. Additional filtering for the local AM263x 3.3V analog power net is done through the LC filter of ferrite-bead FL13 and associated capacitors. This is used to create a low-IR drop low-pass filter that attenuates the higher frequency switching harmonics of the TPS62913RPUR regulator.
Figure 14-12 AM263x controlCARD Excerpt –
3.3V Digital and Analog Power Planes on Layer 5 and Layer 6
Figure 14-13 AM263x controlCARD Excerpt –
3.3V Digital I/O and Analog I/O BGA Pinout and Regulator Output
Figure 14-14 AM263x controlCARD Excerpt –
Common 3.3V Plane Transition Vias
Figure 14-15 AM263x controlCARD Excerpt –
3.3V Digital and Analog Planes Layer 6
Figure 14-16 AM263x controlCARD Excerpt –
3.3V Digital and Analog Power Decoupling Mounting, Layer 10