SPRUHJ1I January 2013 – October 2021 TMS320F2802-Q1 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027-Q1 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F2806-Q1 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1
Another example to introduce the basic elements of SpinTAC Velocity Plan is the agitation stage of a washing machine. The agitation cycle is a basic motion profile. In this example SpinTAC Velocity Plan does not interface to any external sensors or valves and has no conditional transitions. This motion sequence can easily be implemented in SpinTAC Velocity Plan. Figure 14-3 shows the state transition map for the washing machine agitation.
Figure 13-3 State Transition Map of
Example Washing Machine AgitationThe washing machine agitation has two stages: Idle and Wash. The washing machine will stay in the idle state until the start button is pushed. Once the start button is pushed the machine will go into the wash stage where it will agitate between a positive and a negative speed until the washing machine agitation state machine is told to stop.
Figure 14-6 describes the motor velocity during the entire washing machine motion sequence, but it can also be used to describe the motor velocity during the washing machine agitation motion sequence. Refer to the wash stage section of Figure 14-6 and you should see the motor velocity run in the positive direction followed by the negative direction. This represents the washing machine agitation stage.