SPRUJ10E May 2022 – May 2025
The AM263x LaunchPad uses two AM263x SoC inter-integrated circuit (I2C) ports to operate as a controller for various targets. It is important that all I2C data and clock lines are pulled up to the 3.3V system voltage supply to enable communication.
Figure 4-10 I2C Targets| Target | I2C Instance | I2C Addres Bit Description | Device Addressing | LaunchPad Config. | I2C Address |
|---|---|---|---|---|---|
| Board ID EEPROM | I2C1 | The first 4 bits of the device address are set to 1010, the next two are set by the A2 and A1 pins, the seventh bit, a16, is the most significant internal address bit | 0b10110[A2][A1][a16] A1 is connected to 3.3V supply A2 is connected to ground |
0b1010010 | 0x52 |
| LED Driver | I2C1 | The first four bits of the target address are 1100, the following three are determined by A2, A1, and A0 | 0b1100[A2][A1][A0] A2/A1 are connected to ground A0 is connected to 3.3V supply |
0b1100001 | 0x61 |
| BoosterPack Headers | I2C1 | Dependent on target | |||
| BOOTMODE IO Expander | I2C3/TA_I2C | The first 6 bits of the target address are set to 010000, the next bit is determined by the addr pin of the IO expander | 0b010000[ADDR] ADDR pin connected 3.3V supply |
0b0100001 | 0x21 |
| BoosterPack Headers | I2C3 | Dependent on target | |||