Figure 4-2 shows the reset architecture of the AM263x LaunchPad
The AM263x LaunchPad has the following
resets:
- PORz is the Power On
Reset
- WARMRESETn is the warm
reset
Figure 4-3 PORz Reset Signal Tree
The PORz signal is driven by a 3-input
AND gate that generates a power on reset for the MAIN domain when:
- The 3.3V buck converter
(TPS62913) power good output is driven low by having an output voltage that
is below the power-good threshold.
- The 1.2V buck converter
(TPS62912) power good output is driven low by having an output voltage that
is below the power-good threshold.
- The user push button (SW2) is
pressed.
- A P-Channel MOSFET gate's
signal is logic LOW which causes V_GS of the PMOS to be less than zero and
so the PORz signal connects to the PMOS drain which is tied directly to
ground. The signals that can create the logic LOW input to the PMOS gate
are:
- TA_PORZ output from
the Test Automation header
- BP_PORZ output from
either of the BoosterPack sites.
The PORz signal is tied to:
- AM263x SoC PORz input
- BOOTMODE State Driver's
output enable input
- There is an RC filter
to create a 1ms delay from GND to 3.0V such that the SOP State
Driver's output enable input is low longer than the required SOP
hold time following a PORz de-assertion.
There is a Test-Automation PORz
Override header that enables the ability to hold TA_GPIO3 low when a jumper is
installed. This enables the BOOTMODE Control from the Test Automation Header.
Figure 4-4 WARMRESETn Reset Signal
Tree
The WARMRESETn signal creates a warm
reset to the MAIN domain when:
- The user push button (SW3) is
pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_RESETz) to a P-Channel MOSFET gate which
causes V_GS of the PMOS to be less than zero and so the RESETz signal
connects to the PMOS drain which is tied directly to ground.
The WARMRESETn signal is tied to:
- AM263x SoC WARMRESETN
output
- RESETN_PB signal that is
created from push button + PMOS logic
- Micro SD Load Switch control
input via a 2 input AND Gate with an AM263x SoC driven GPIO signal
(GPIO122)
- Both Ethernet PHY's reset
input
The AM263x LaunchPad also has an
external interrupt to the SoC , INT1, that occurs when:
- The user push button (SW4) is
pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_GPIO1) to a P-Channel MOSFET gate which
causes V_GS of the PMOS to be less than zero and so the INTn signal connects
to the PMOS drain which is tied directly to ground.