SPRUJF0 August   2025 F28E120SB , F28E120SC , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1

 

  1.   1
  2.   TMS320F2802x/TMS320F2803x to TMS320F28E12x Migration Overview
  3.   Trademarks
  4. 1 Introduction
    1. 1.1 Abbreviations
  5. 2 Central Processing Unit (CPU)
  6. 3 Development Tools
    1. 3.1 Driver Library (Driverlib)
    2. 3.2 Migrating Between IQ_Math and Native Floating-Point
    3. 3.3 Embedded Application Binary Interface (EABI) Support
  7. 4 Package and Pinout
  8. 5 Operating Frequency and Power Management
  9. 6 Power Sequencing
  10. 7 Memory Map
    1. 7.1 Random Access Memory (RAM)
    2. 7.2 Flash and OTP
      1. 7.2.1 Size and Number of Sectors
      2. 7.2.2 Flash Parameters
      3. 7.2.3 Entry Point into Flash
      4. 7.2.4 Dual Code Security Module (DCSM) and Password Locations
      5. 7.2.5 OTP
      6. 7.2.6 Flash Programming
    3. 7.3 Boot ROM
      1. 7.3.1 Boot ROM Reserved RAM
      2. 7.3.2 Boot Mode Selection
      3. 7.3.3 Bootloaders
  11. 8 Architectural Enhancements
    1. 8.1 Clock Sources and Domains
    2. 8.2 Dual-Clock Comparator (DCC) Module
    3. 8.3 Watchdog Timer
    4. 8.4 Peripheral Interrupt Expansion (PIE)
    5. 8.5 Lock Protection Registers
    6. 8.6 General-Purpose Input/Output (GPIO)
    7. 8.7 External Interrupts
    8. 8.8 Crossbar (X-BAR)
  12. 9 Peripherals
    1. 9.1 New Peripherals
      1. 9.1.1 Direct Memory Access (DMA)
      2. 9.1.2 Analog Subsystem Interconnect
      3. 9.1.3 Comparator Subsystem (CMPSS)
      4. 9.1.4 Programmable Gain Amplifier (PGA)
    2. 9.2 Control Peripherals
      1. 9.2.1 Enhanced Pulse Width Modulator (MCPWM)
      2. 9.2.2 Enhanced Capture Module (eCAP)
      3. 9.2.3 Enhanced Quadrature Encode Pulse Module (eQEP)
    3. 9.3 Analog Peripherals
      1. 9.3.1 Analog-to-Digital Converter (ADC)
    4. 9.4 Communication Peripherals
      1. 9.4.1 SPI
      2. 9.4.2 SCI
      3. 9.4.3 UART
      4. 9.4.4 I2C
  13. 10Emulation – JTAG Port
  14. 11Silicon Errata
  15. 12Device Comparison Summary
  16. 13References

Crossbar (X-BAR)

The X-BARs provide a flexible means for interconnecting multiple inputs, outputs, and internal resources in various configurations. The F28E12x device contains three X-BARs: the Input X-BAR, the Output X-BAR, and the PWM X-BAR.

  • Input X-BAR – is used to route external GPIO signals into the device. It has access to every GPIO pin where each signal can be routed to any or multiple destinations which include the ADCs, eCAPs, PWMs, Output X-BAR, and external interrupts. The F28E12x Input X-BAR has sixteen inputs (INPUT1 through INPUT16) and any of the sixteen inputs can be selected as an external input to each of the eCAP modules.
    Note: This differs from the F2802x/03x devices which uses the GPIO multiplexer to select a specific dedicated input pin to access the eCAP module.
  • Output X-BAR – is used to route various internal signals out of the device. It contains eight outputs that are routed to the GPIO structure, where each output has one or multiple assigned pin positions, which are labeled as OUTPUTXBARx. Additionally, the Output X-BAR can select a single signal or logically OR up to 32 signals.
  • PWM X-BAR – is used to route signals to the MCPWM Digital Compare submodules of each MCPWM module for actions such as trip zones and synchronizing. It contains eight outputs that are routed as TZx signals to each MCPWM module. Likewise, the MCPWM X-Bar can select a single signal or logically OR up to 32 signals.