SPRUJF0 August   2025 F28E120SB , F28E120SC , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1

 

  1.   1
  2.   TMS320F2802x/TMS320F2803x to TMS320F28E12x Migration Overview
  3.   Trademarks
  4. 1 Introduction
    1. 1.1 Abbreviations
  5. 2 Central Processing Unit (CPU)
  6. 3 Development Tools
    1. 3.1 Driver Library (Driverlib)
    2. 3.2 Migrating Between IQ_Math and Native Floating-Point
    3. 3.3 Embedded Application Binary Interface (EABI) Support
  7. 4 Package and Pinout
  8. 5 Operating Frequency and Power Management
  9. 6 Power Sequencing
  10. 7 Memory Map
    1. 7.1 Random Access Memory (RAM)
    2. 7.2 Flash and OTP
      1. 7.2.1 Size and Number of Sectors
      2. 7.2.2 Flash Parameters
      3. 7.2.3 Entry Point into Flash
      4. 7.2.4 Dual Code Security Module (DCSM) and Password Locations
      5. 7.2.5 OTP
      6. 7.2.6 Flash Programming
    3. 7.3 Boot ROM
      1. 7.3.1 Boot ROM Reserved RAM
      2. 7.3.2 Boot Mode Selection
      3. 7.3.3 Bootloaders
  11. 8 Architectural Enhancements
    1. 8.1 Clock Sources and Domains
    2. 8.2 Dual-Clock Comparator (DCC) Module
    3. 8.3 Watchdog Timer
    4. 8.4 Peripheral Interrupt Expansion (PIE)
    5. 8.5 Lock Protection Registers
    6. 8.6 General-Purpose Input/Output (GPIO)
    7. 8.7 External Interrupts
    8. 8.8 Crossbar (X-BAR)
  12. 9 Peripherals
    1. 9.1 New Peripherals
      1. 9.1.1 Direct Memory Access (DMA)
      2. 9.1.2 Analog Subsystem Interconnect
      3. 9.1.3 Comparator Subsystem (CMPSS)
      4. 9.1.4 Programmable Gain Amplifier (PGA)
    2. 9.2 Control Peripherals
      1. 9.2.1 Enhanced Pulse Width Modulator (MCPWM)
      2. 9.2.2 Enhanced Capture Module (eCAP)
      3. 9.2.3 Enhanced Quadrature Encode Pulse Module (eQEP)
    3. 9.3 Analog Peripherals
      1. 9.3.1 Analog-to-Digital Converter (ADC)
    4. 9.4 Communication Peripherals
      1. 9.4.1 SPI
      2. 9.4.2 SCI
      3. 9.4.3 UART
      4. 9.4.4 I2C
  13. 10Emulation – JTAG Port
  14. 11Silicon Errata
  15. 12Device Comparison Summary
  16. 13References

Dual Code Security Module (DCSM) and Password Locations

The DCSM offers protection for two zones (zone-1 and zone-2), and is intended to block access and visibility to the various on-chip memory resources with the purpose of preventing duplication and reverse engineering of proprietary code. The options for both zones are identical, and each memory resource can be assigned to either zone. Either zone can protect each sector of flash individually, each LSx memory block individually, User OTP, and secure ROM.

Each zone is secured by its own 128-bit (four 32-bit words) user defined CSM password, which is stored in its dedicated OTP location based on a zone-specific link pointer. The user accessible CSMKEY registers are used to secure and unsecure the device, and a new or un-programmed device is unlocked by default. Since the OTP cannot be erased, flexibility is provided by using a link pointer to select the location of the active zone region within the OTP block, allowing the user to make multiple modifications to the configuration up to thirty times. This is accomplished by exploiting the fact that each bit in the OTP can be programmed one bit at a time, and a “1” can be programmed to a “0”, but not erased back to a “1”. The most significant bit position in the link pointer that is programmed to a “0” defines the valid offset base address for the active zone region within the OTP block. This differs from the F2802x/03x devices where the 128-bit (eight 16-bit words) password is stored in the last eight locations in flash.