SPRUJF0 August 2025 F28E120SB , F28E120SC , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1
This section highlights the boot ROM enhancements of the F28E12x device. The boot ROM has increased in size to 64K x 16 words on F28E12x from 8K x 16 words on F2802x/03x. The F28E12x boot ROM origin address starts at 0x003F 0000 and contains the contents of Table 7-4.
| Boot ROM Contents |
|---|
| Zone 1 Secure Flash Boot |
| Zone 1 CRC Code |
| ROM Signature |
| Version |
| FPU32 Fast Tables |
| FPU32 Twiddle Tables |
| Boot Code |
| Flash API Tables |
| AES Tables |
| RTS Lib |
| IQmath Table |
| Interrupt Handlers |
| Vector Table |
In order to take advantage of the F28E12x FPU, the boot ROM contains floating-point math tables which are used by the C28x FPU Fast RTS Library, located in C2000Ware at (C2000Ware → libraries → math → FPUfastRTS). For additional information about the boot ROM, see the F28E12x Microcontrollers Technical Reference Manual.