SPVA018 August 2025 LM2904B
Knowing the internal protection scheme of the op amp is important, because the information helps when designing protection schemes for the system as a whole. ESD diodes are designed for out of circuit events, so additional design consideration is needed if wanting to optimize your system for any in circuit electrical overstress events (EOS).
Consider Figure 5-1. This op amp has the diode to supply protection scheme, with an LDO attached to the positive supply. The max supply of the op amp is 10V, and the LDO is regulating 24V to 5V. 15V is applied to the non-inverting node of the op amp.
D3 directs the voltage through the device into the power supply; since the voltage is above the absolute maximum rating, the absorption device turns on. However, the voltage being supplied is continuous, so the absorption device latches and stays on unless the circuit is power cycled. While the circuit is on, the absorption device is drawing large amounts of current from the LDO, generating a large amount of heat and oftentimes destroying the device.
How can this be prevented from happening? There are two simple steps to take. One is to add an input resistance. The next step is to add a TVS diode to the power supply.