SPVA018 August   2025 LM2904B

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2ESD Overview
    1. 2.1 What is Electrostatic Discharge?
      1. 2.1.1 ESD Cell Robustness in Semiconductors
  6. 3Types of ESD Cells
    1. 3.1 Dual Diode Configuration
      1. 3.1.1 Why Not Always Use Dual Diode Configuration?
    2. 3.2 Bootstrapped Diodes
    3. 3.3 Absorption Devices
      1. 3.3.1 Active Clamps
      2. 3.3.2 GCNMOS Clamps
    4. 3.4 Silicon Controlled Rectifiers
    5. 3.5 CER and ECR NPN Diodes
      1. 3.5.1 Measuring the Response of an ECR and CER ESD Cell
    6. 3.6 Comparison of ESD Cells
  7. 4How to Determine the ESD Structure of the Device from the Data Sheet
  8. 5How to Protect The System from In Circuit ESD/EOS Events
    1. 5.1 Using TVS Diodes and Series Resistance for Circuit Protection
    2. 5.2 Using Schottky Diodes for Circuit Protection
  9. 6How to Test an Op Amp in a System Level Circuit
    1. 6.1 ESD Protection Cell Advancements Over the Years
  10. 7Summary
  11. 8References

Dual Diode Configuration

Figure 3-1 shows the most common ESD protection structure for an op amp. Dual diodes are placed on the inputs and outputs and are routed to the supplies. The ESD diodes direct any ESD transients onto the power supply. For this reason, the diodes are often called ESD steering diodes. To prevent damage to the op amp supply, an ESD absorption device is placed across the supply. The absorption device triggers on and act as a low impedance when the ESD event occurs. Thus, the absorption device limits the voltage applied across the supply and protect the device.

 Dual Diode Configuration on Op Amp
                Input and Output Figure 3-1 Dual Diode Configuration on Op Amp Input and Output

The benefits of the dual diode configuration include low leakage and low capacitance, making the dual diode configuration a great option for most op amps. The diodes only take up a small area, and are preferred to handle high frequency inputs and outputs. However, there are certain scenarios in which the dual diode configuration is not designed for protection.