SPVA018 August 2025 LM2904B
Like any semiconductor technology, great advancements have been made over the decades. ESD protection was not a standard part of the op amp design until the 1990s. Thus, many devices from the 1970s and 1980s possibly does not have ESD cells! These older generation op amps have larger geometry devices so the op amps are inherently more robust against ESD damage. However, if ESD protection is the main concern, review the ESD specification and confirm that the device meets your requirement.
Some op amps have been updated over the years, moving to newer processes and technologies. During this modernization, ESD cells were added or changed. Since the topology has changed, the inherent resistance from the diode structure is also different. This can lead to false failures in a system level board test.
Most diodes follow the same general IV curve, as seen below. Usually, the forward bias voltage is around 0.7V for silicon diodes. However, all diodes vary, and updating the ESD cells can change the IV curve characteristics of ESD cells inside an op amp.
One example of an op amp with updated ESD structure is the OPAx130 family. Table 6-1 shows the IV measurement differences of the op amp with the original ESD design, and the updated design. In this setup, 100µA is forced into the pin, and the voltage is measured.
| Pin to V+ Voltage Measurements | Pin 1 to Pin 8 (OUT A to V+) | Pin 2 to Pin 8 (-IN A to V+) | Pin 3 to Pin 8 (+IN A to V+) | Pin 5 to Pin 8 (+IN B to V+) | Pin 6 to Pin 8 (-IN B to V+) | Pin 7 to Pin 8 (OUT B to V+) |
|---|---|---|---|---|---|---|
| OPA2130 Original Design | 0.609678V | 0.699382V | 0.668025V | 0.670190V | 0.668482V | 0.610322V |
| OPA2130 Redesign | 0.688358V | 0.709175V | 0.709203V | 0.709174V | 0.709235V | 0.688545V |
Note that while the diode structure of a device can change, there is no change in behavior of the device. This is because these protection structures are only triggered during abnormal device operation, such as ESD.