SPVA018 August 2025 LM2904B
The CER/ECR NPN ESD protection structure is another common option, particularly for higher voltages. This behaves similarly to a snapback diode, in that the voltage reaches a certain level before dropping back to the threshold voltage. Figure 3-9 shows the general layout.
The protection structure raises the base potential to lower the NPN trigger voltage. These are preferred when the device is tolerant to a high trigger or clamping voltage. Note that one pad is connected to ground through a diode. The other pad is voltage triggered. This offers ESD protection while taking up a relatively small area, albeit not as small as an SCR structure. These structures are also advantageous because the structures are generally considered to be a latch-up free design unlike SCRs, which are more prone to latch-up.