SPVA018 August 2025 LM2904B
How can you know what type of protection the op amp has? The effectiveness of the ESD protection is listed on the data sheet in the ESD ratings table. This specification is developed by applying an emulated ESD pulse to all the device pins and checking for damage. The ESD event is generated by special test equipment that creates a controlled ESD pulse with the same charge, voltage levels, inductance, resistance, and capacitance of a real-world situation. Typically, the real-world situation being emulated is the human-body or charged-device in contact with a low impedance. This was mentioned earlier in a previous section. The ESD voltage levels specified in Table 4-1 reflect the maximum ESD voltage that was applied without damaging the device TLV9141.
| VALUE | UNIT | ||||
|---|---|---|---|---|---|
| V(ESD) | Electrostatic discharge | Human-body model (HBM), per ANSI/ESDA/JEDEC JS-001 (1) | ±4000 | V | |
| Charged-device model (CDM), per ANSI/ESDA/JEDEC JS-002 (2) | ±1500 | ||||
There are two ways to know if a particular device contains ESD protection diodes or relies upon another method to achieve ESD robustness. Look at the Absolute Maximum Ratings table, or in some cases you can find a functional block diagram that illustrates the diodes. In the Absolute Maximum Ratings table, when the input voltage range is limited to approximately 0.5V beyond the supply range, then the device contains dual diode configuration ESD diodes (see Table 4-2). This is due to the forward bias voltage of a diode generally being around 0.5V. If the input signal stays inside this range the ESD diodes does not turn on. This type of protection generally also provides an input current limit of ±10mA.
| MIN | MAX | UNIT | |||
|---|---|---|---|---|---|
| VS | Supply voltage, VS = (V+) – (V–) | 26 | V | ||
| Input voltage | Common-mode | (V–) –0.5 | (V+) + 0.5 | V | |
| Differential | (V+) – (V–) + 0.2 | ||||
| Output short-circuit (1) | Continuous | ||||
| TJ | Operating junction temperature | -40 | 150 | °C | |
| Tstg | Storage temperature | -65 | 150 | °C | |
If the device is using a transient or level triggered protection, the input voltage range usually goes up to the maximum recommended power supply voltage operating conditions. This is shown below using the LM2904B data sheet (see Table 4-3).
| MIN | MAX | UNIT | ||||
|---|---|---|---|---|---|---|
| Supply voltage, VS = ([V+] – [V–]) | 40 | V | ||||
| Differential input voltage, VID(2) | –32 | 32 | V | |||
| Input voltage, VI | Either input | –0.3 | 40 | V | ||
| Duration of output short circuit (one amplifier) to V–
at (or below) TA = 25°C, VS ≤ 15V (3) |
Unlimited | s | ||||
| Operating ambient temperature, TA | –40 | 125 | °C | |||
| Operating virtual-junction temperature, TJ | 150 | °C | ||||
| Storage temperature, Tstg | –65 | 150 | °C | |||
3) Short circuits from outputs to the supply pins can cause excessive heating and eventual destruction.
Another simple way to determine the internal ESD protection scheme is to look at the functional block diagram of the device. The data sheet often contains this, and the internal diodes are frequently included in the functional block diagram. This was previously seen from Figure 3-2, the functional block diagram for OPA928.