SPVA018 August 2025 LM2904B
Silicon controlled rectifiers, or SCRs, are another common option used for clamping. SCRs leverage hole generation at the drain of the MOSFET to increase the base current of the NPN. This has a cascading effect, and in turn, increases the current in the parasitc PNP, leading to regeneration. SCRs leverage a cascading PNP/NPN device structure for ESD protection. The SCR has a low holding voltage (VH), but high trigger voltage (VT), which creates a deep snapback effect. This effect can be clearly seen in an IV curve (Figure 3-7). Figure 3-8 is a high level design figure of a typical SCR.
SCRs are often used in designs where area is a key parameter, due to the small size. SCRs also have very low leakage and capacitance, providing further advantage to designs with low bias current. However, these ESD cells have a higher risk of latch-up, since the holding voltage of the cell is lower than VDD. Latch up occurs when there is positive feedback between the NPN/PNP. If latch up does occur in your device, best practice is to power cycle to prevent damage to the device.