TIDUE74F April 2018 – March 2026
During the TRANSMIT_DATA (or SEND_DATA) state, the encoder interface sends the request to the encoder. The request is sent from the SPI TX FIFO on the falling edge of the SPICLK. During TRANSMIT_DATA, the CLB:
The number of CLB_SPI_CLOCKs required to send the transmission was loaded into both the match1 and match2 of the CLOCK_COUNT by the C28x during command setup.
Refer to: Figure 2-2, marker (2).
When the required number of clocks has been reached, the CLOCK_COUNT_COMPLETE (match2) and TRANSMIT_COMPLETE (match1) signals are pulled high. The effect is: