TIDUF18A October 2022 – February 2024
Figure 5-56 shows CLLLC operation at 19 A (6.6 kW) under the following parameters:
Figure 5-56 CLLLC Operation 19 A (6.6 kW)Figure 5-57 shows CLLLC operation at 10 A and the following parameters:
Figure 5-57 CLLLC Operation 10 AA zoom-in of the GaN switch drain-to-source voltage transition is shown to be approximately 40 ns in Figure 5-58. This rapid transition comes from the low COSS of the LMG3522.
The waveform in Figure 5-58 is measured using the following parameters:
Figure 5-58 CLLLC Operation 10 A - GaN FET TransitionsThe waveform in Figure 5-59 is measured using the following parameters:
Figure 5-59 CLLLC Operation 2 AA zoom-in of the GaN switch drain-to-source voltage transition is shown to be approximately 75 ns in Figure 5-60. This rapid transition comes from the low COSS of the LMG3522. The slightly longer transition time in this image comes from the lighter load condition and the resulting reduced current flow.
The waveform in Figure 5-60 is measured using the following parameters:
Figure 5-60 CLLLC Operation 2 A - GaN FET Transitions