TIDUF18A October 2022 – February 2024
Compensation Designer launches. PI-based controller can be tuned from a pole zero perspective to ensure stable closed loop operation. Stability of the system when using the designed compensator can be verified by observing the gain and phase margins on the open loop transfer function plot in the Compensation Designer, as shown in Figure 5-33.
Figure 5-33 Current Loop Design Using Compensation DesignerOnce satisfied with the open loop gain, the compensator values can be updated in the ttplpfc_settings.h file.
Close the Compensation Designer