TIDUF18A October 2022 – February 2024
Figure 5-25 SFRA Open Loop Plot
for the Closed Current Loop (Vprim 400 V, Vsec 300 V, Power 1.972 kW,
Lab 4)The Frequency Response Data is also saved in the project folder, under an SFRA Data Folder, and is time-stamped with the time of the SFRA run.
The data matches closely to the designed compensator, but it is reasonable to expect deviations because the measurement in open loop is susceptible to error due to small signal injection which can drift the DC point of the converter.
Test the SFRA at different current set points, making sure the period is not clamped, to verify that the system is stable across the operable range.
, or by using Target →
Halt. Then, take the MCU out of real-time mode by clicking the
. Finally, reset the MCU
.
(Target → Terminate all).