TIDUFE9 August 2025
Rogowski coils are di/dt sensors measuring the rate of change of current rather than the current. As a result, Rogowski coils are highly sensitive to rapid transients and switching noise, especially near the zero-crossing point of the current waveform. At zero crossing, the current (i) is momentarily at zero leading to sharp voltage spikes and high-frequency ringing at the output of the coil. Zero crossing spikes and ringing can distort the signal and introduce non-linearity in the signal chain.
To address the zero crossing issues and non-linearity, a low-pass filter is implemented at the input of the differential amplifier. The purpose of the low-pass filter is to attenuate high-frequency components, including the unwanted spikes and ringing, thereby improving signal integrity and making the system behave more linearly.