TIDUFE9 August 2025
Gain selection of the gain amplifier is only controlled by using a single resistor (RG). Resistor RG connects to pin 1 and pin 8 of the INA828 device. This resistor must be as close as possible to the pins of the amplifier to reduce the line capacitance between pin 1 and pin 8. The gain of the amplifier must be set correctly according to:
where
S = sensitivity of the coil (measured in μV)
Imax = the maximum current that is flowing through the conductor
L = limit of the analog input pins of the ADC
Gs = gain of the system
where
To set the gain to the correct value, sensitivity and maximum current must be known.