SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Descriptor starvation occurs when the Port needs to fetch a free descriptor from the RX ring and none are available. When the port detects that descriptor starvation has occurred it will react based on the value of the rx_error_handling bit which was programmed into the Rx Flow N Configuration Register A (<RFLOW[a]_RFA> [28] RX_ERROR_HANDLING).
If the rx_error_handling bit is cleared:
The Port will increment an internal per-channel starvation counter and will then flush the packet.
If the rx_error_handling bit is set:
The Port will assert a RX descriptor starvation event (which may cause an interrupt to the Host) and will then wait for the doorbell for the selected flow to be written with a positive value. Note that the intention is that the port will wait for an entry to be added to the ring. It is assumed that when in this mode, if data loss is not desired that the host will guarantee that a chain of buffers will be provided that can receive the entire packet.