SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The MCASP includes error-checking capability for the serial protocol and data underrun. In addition, the MCASP includes a timer that continually measures the high-frequency controller clock every 32 AHCLKX clock cycles. The value of the timer can be read to get a measurement of the clock frequency and has a minimum and maximum range setting that can set an error flag if the controller clock goes out of a specified range.
When one or more errors (software selectable) are detected, an interrupt can be generated if desired, based on one or more error sources.