DLPU101C december 2020 – may 2023 DLPC900
When deleting images from flash, the flash device is erased and then updated with the firmware that contains the new images. In the event the flash is accidentally corrupted, follow the instructions under JTAG Flash Programming (see Section 7.11) to reload the original firmware. To remove accidental erasing or corruption of the flash device, it is recommended to operate in Pattern On-The-Fly Mode.
The user must exercise caution when selecting the correct firmware file. Ensure that firmware file is version 3.0 or later. Using version 2.0 or earlier renders the EVM inoperable. Version 6.0 or later is recommended.
Follow these steps to begin deleting images from the firmware file:
The updated firmware file has no images. It is advisable to rename the updated firmware file with a specific name so that later it can be reused as a firmware file that has no images.