The bitmap images to be added to the firmware file
must have the native resolution of the DMD that is being used. The GUI
returns an error if it encounters an incorrect image size. Please be sure any images
you add to the firmware are of the correct resolution.
- Continuing from the previous set of steps, click the Browse button and
select the firmware file in step 8 or the renamed version.
- Select Pre-Stored Pattern Mode from the Operating Mode group box.
The Pattern Mode panel is displayed.
- In the menu bar click the Load button and select add_72.txt. The
file is typically stored in the folder named C:\Texas
Instruments-DLP\DLPC900REF-SW-x.x.x\DLPC900REF-GUI\Images and Batch
files\, then LCR[DMD]_Images\ folder depending on
which DLPC900 DMD EVM is being used. Be sure to select the correct file for the
DMD EVM being used. This file adds 72 1-bit images to the Pattern Design
panel. See Figure 7-10.
- Click the Select All Patterns button from Menu bar to select all the images.
- Under Bit Information select bit depth 1 for all images.
- Enter 120000 µs for the exposure time for all images.
- Enter 10000 µs for the dark time for all images.
- Select color Red for all images.
- Click the Firmware button at the top of the GUI.
- Under Batch File check the box next to Add Patterns Images and
Clear Existing Patterns. These patterns are from the Pattern
Design panel. See Figure 7-10.
- Under power up defaults update the firmware tag (ex:
dlp6500_6.0.0_72images)
- Click the Update Firmware button.
- The GUI displays a pop-up box providing the name of the updated firmware
file.
- Click the Browse button and select the firmware file from step 12.
- Click the Upload button and allow firmware to be uploaded to the flash
memory.
Note:
When a firmware file is
uploaded, a cached version of that file is created on the PC in its
original folder location in a subdirectory named
FlashLoaderCache. Each time a new firmware is uploaded the GUI
compares it to the cache file on the PC and only reprograms the new
sectors. The cache file is then updated to represent the latest firmware
image. Caching leads to significant download speed improvements if the
new firmware and the previous firmware are similar.
Note:
If a full
reprogramming of the flash is desired, delete the
FlashLoaderCache folder or select a firmware image
from a different file location that does not have a cached
firmware. Programming the firmware to a different board requires
deleting the FlashLoaderCache.
- Once the EVM resets and displays a solid curtain, click the Pre-Stored
Pattern Mode from the Operating Mode group box.
- The Pattern Design panel (See Figure 7-10) is displayed which includes the pattern images that were added into the
panel in step 3 with all the settings from steps 5-8. If the Pattern
Design panel is not displayed, then click the Pattern Mode button
at the top of the GUI. Press Stop if pattern sequence is currently
playing.
- Click the Update LUT button.
- Click the Start button.
- All 72 1-bit images are displayed with the settings that were entered in steps
5-8.
It is possible to add many images to the firmware
without deleting all the images that are currently in the firmware, and then select
which images and bit positions to choose for different pattern sequences. To do this
requires editing the image index and the bit position in the Pattern LUT
Definition that is sent to the EVM, and then using the Batch File
method to upload the Pattern LUT Definition and Configuration settings
to the EVM.
The following example shows how to choose
different images and bit positions from the 72 1-bit images that are stored in the
firmware.
Follow these steps to edit the image index and bit position of the images to be used for the pattern sequence.
- Stop the pattern sequence if it is currently running.
- Delete all images except for the first two in the Pattern Design panel. See Figure 7-10.
- Select the first image and set the color to Yellow.
- Select the second image and set the color to Green.
- Click the Batch File button at the top of the GUI.
- Check the Enable Command Logging box, and then click the Clear All button.
- Click the Pattern Mode button at the top of the GUI.
- Click the Update LUT button.
- Click the Batch File button at the top of the GUI.
- Figure 7-21 shows the Pattern LUT Definition and Configuration of the pattern sequence.
- Click the Save Batch File button to save the contents to a file.
- Click the Pattern Mode button at the top of the GUI.
- Click the Start button and take note of the images that are displayed, and then Click the Stop button.
- Click the Batch File button at the top of the GUI.
- Click the Clear All button and uncheck the Enable Command Logging box.
- Use Notepad or a similar editor to open and edit the batch file saved in step
11. The file is typically stored in the folder named C:\Texas
Instruments-DLP\DLPC900REF-SW-5.2.0\DLPC900REF-GUI\Images and Batch
files\, then LCR[DMD]_Images\ folder depending on
which DLPC900 DMD EVM is being used. Change the image index and bit position as
seen in Figure 7-22. See the DLPC900 Programmer’s Guide (DLPU018)
for details of the Pattern LUT Definition and Configuration commands.
- Figure 7-22 shows the image index and the bit position of the images for the two patterns, where the values have been changed compared to the values in Figure 7-21. Click the Save to save the new batch file.
- In the Batch File tab click the Clear All button, and then click the Load Batch File button and load the file from step 17.
- Click the Execute All button.
- Click the Pattern Mode button at the top of the GUI.
- Click the Start button.
Notice that two different images or bit positions are displayed compared to the images in step 13.
Therefore, many different images can be added to the firmware and knowing the image index and the bit positions of each image, the user can create different Pattern LUT Definition and Configuration batch files that select different images and bit positions from the images stored in the firmware.