Input triggers have some special considerations when using the new Edit LUT Feature. As previously noted, Pattern 3 (“Matt”) has an input trigger associated with it. When a trigger is added to a pattern, the pattern preceding it, Pattern 2 (“Sue”) in this case, has an all-black pattern loaded at the very end of it so that while the sequence is waiting for the trigger it does not have a pattern displaying during the wait. This attribute follows Pattern 2 during a reorder. In our example the first entry (Pattern 2) in the new display order has a 105 µs dark pattern at the end of it. If Pattern 0 ("Bob") is placed in front of Pattern 3 ("Matt" - the triggered pattern) then the last bit-pattern of Pattern 0 (“Bob”) continues to display in our new display order while waiting for the trigger in Pattern 3 (“Matt”).
The unwanted trigger behavior can be compensated for by one the following methods:
- Method 1: Consider Pattern 2 and 3 ("Sue" and "Matt") as a set that must always be moved together in your new display order.
- - Method 1 is the simplest, but the tradeoff is that these two patterns are not separable without the undesired trigger behavior described above.
- Method 2: Add a 1-bit all-black pattern with the shortest duration allowed for most DMDs preceding the trigger pattern. See Minimum Exposure in Any Pattern Mode in the DLPC900 Programmer's Guide for details. Now consider this pattern and the triggered pattern following it as a set that must always be moved together.
- - Method 2 is more versatile, but the pattern set must always contain a triggered pattern.
- Method 3: Add a 1-bit all-black pattern with the shortest duration allowed followed by a triggered 1-bit all-black pattern, and remove the trigger from the actual pattern of interest. These two patterns are now a versatile trigger set that can be used repeatedly wherever a trigger is desired. Note that since the triggered pattern is black, even if your exposure integration begins with the triggered black pattern there is no light contributing to your exposure.
- - Method 3 is the most versatile since this standalone trigger set only has to be placed in the Pattern Index set (on the Pattern Mode page) once but can be used in many positions when defining a new display order.